Other Parts Discussed in Thread: UCC27524, UCC27531
Hi
I've been thinking to use the UC3709 MOSFET driver to drive the ultrasonic atomizer transducer to create a mist/humidifier.
As going through driver IC, seems that IC can support a max of 40V. Is there any other driver which could support a higher voltage?
Ultrasonic atomizer transducer specs as below,
Resonant freq-1.7MHz
Capacitance-1500pF
The voltage on the transducer peak to peak- 110V(MAX).