Other Parts Discussed in Thread: BQ25120, BQ25120A
Hello,
We have a wrist-worn device in the final phases of development, but our BQ25121A is experiencing a severe issue holding us back from going to market. The device enters, what our testers call, "Brick Mode" under the following conditions:
1. If the BQ25121A enters ship mode.
2. If the battery discharges to VBAT < BUVLO.
To exit "Brick Mode," holding down MR or toggling it doesn't work, plugging the device in doesn't work either. The only way to exit "Brick Mode" is by detaching and reattaching the battery.
Observations while bricked:
VBAT = 4.0v
PMID = 4.0v
SW = 0v
LDO = off
Since both Ship Mode and battery discharge below BUVLO disconnects the battery with an internal FET, we believe that's where the problem lies. When in Ship Mode, the device should disconnect the battery thus PMID should also be 0v. We believe that the device is failing at this point, crashes, and doesn't respond or wake-up to MR or VIN.
This "Brick Mode" state has been on this forum before, although with the BQ25120 and BQ25120A. The forum links are below, I do not see this issue being resolved so we cannot fix based on those forum posts.
Thank you, in advance, for your assistance.
Keith Creedy