Dear TI-Team
The attached circuit (see above) shows a very special behaviour. It is already on a PCB and we try to run it by applying 24V at 24V_IN. Except for the On/Off button nothing else is connected to the board.
Once the MAIN_SWITCHED is being turned on by pressing the button, the Mosfet (Q5) switches a few times (3-4) before it stays closed. The gate is driven by the Pin DR of U2 and seems to aim this functionality. If we give 24V and allow more than 1.5A current Q5 simply burns thru (happened once already).
According to our simulation in Webench (see below) it should work just fine.
- Removing R25 didn't help (removing the lowpass filter)
- increasing R27 to 75mOhm didn't help (reducing the maximum allowed output current).
- The load itself at 24V_MAIN seems to be fine. Applying 24V_MAIN directly worked perfectly with very little current consumption.
We run out of ideas what to look for. Thank you very much in advance for your help!
Best regards,
Ivan