Hello,
I have a question regards the external clock in parallel operation with two LMZ31710 deivces. According to the Application Report SNVA695 "The clock must be present before input power is applied", but in my case I don't have a clock unless this switcher runs and generate the low voltage rail. So the question is what happens if I apply the clock after the parts are running? I intend to apply external clock only to the master and let the slave run off the Sync_Out of the master.
In my previous design which uses only one LMZ31710, I also apply the clock after the part runs up and generates the voltage rail which powers the clock circuit and it seems to run fine, I have to mention that I apply the clock through an AC coupling circuit.
Thanks in advance!