Hi TI-team
Can I use Hybrid dimming when I have PWM input?
When using PWM input, does it mean that the LED turns on and off with the duty cycle of PWM in put for the current set in ISET?
Best Regards,
Koji Hayashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI-team
Can I use Hybrid dimming when I have PWM input?
When using PWM input, does it mean that the LED turns on and off with the duty cycle of PWM in put for the current set in ISET?
Best Regards,
Koji Hayashi
You could use Hybrid dimming when you have PWM input.
Correct for your second question.
You could use Hybrid dimming when you have PWM input.
Correct for your second question.
Hi Charles-san
Thank you for quick response.
In the case of hybrid dimming, PWM input: 200Hz, LED PWM: 152Hz, if I want to brighten the LED by 1 bit, should I set the duty cycle of the PWM input at 0.016% since 0001h is approximately 803ns?
200Hz=5ms
803ns/5ms*100=0.016%
Sorry, I misunderstood.
803ns/5ms*100=0.016%
803ns/6.58ms(1/152Hz)*100=0.000122%
Do you mean the brightness of 0001h when the duty cycle of PWM input is 0.000122%?
Hi Koji-san,
If you want to increase 1 bit output duty cycle, the PWM duty cycle increase step is 1/65536*1/200.
Hi Charles-san
Thank you for response.
I understand.
I understood that the LED is divided into 65536 by the Duty of the PWM input and dimmed.
If it is 50%, it will be dimmed as 32768/65536:8000h.
Other questions have come up, so I'll ask them in a separate thread.
Best Regards,
Koji Hayashi