This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC33063A: Power consumption in idle mode

Part Number: MC33063A

Hello,

I need help to reduce power consumption of the attached MC33063A Circuit.

I am measuring current as shown in the image and it is ~6-7mA. No load condition.

Nothing else is connected except relay coil positive terminal at +12V. Relay is OFF.

Rectifier Output: 32VDC

Is the 6-7mA current consumption expected when there is no load except 5V LDO connected at it`s output?

Any help on this circuit would be really helpful.

Thanks