Hi TI experts,
A customer inquired for a solution to charge Li/SOCL2 battery.
Are there any items available to TI? Attached the battery specification sheet.
Specification_VEL13353R8257G (3.8V 250F).pdf
Please check it.
Thanks,
Downey Kim.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI experts,
A customer inquired for a solution to charge Li/SOCL2 battery.
Are there any items available to TI? Attached the battery specification sheet.
Specification_VEL13353R8257G (3.8V 250F).pdf
Please check it.
Thanks,
Downey Kim.
Hi Downey,
From the spec it look like this cell follows a CCCV curve of 2.5 - 3.8V. BQ21062 may be OK, you can set the charging voltage to 3.8V. The min precharge threshold is 2.8V. So you would be charging at the precharge value between 2.5-2.8V (77.5mA max).
I don't think we have any stand alone device that would work here.
Best regards,
Nick
Hi Downey,
I think we need to confirm with the battery manufacturer that this battery is, in fact, rechargeable after initial charge during production. If I search on Li/SOCL2 batteries (actually closer to supercaps), most say they are primary (non-rechargeable) the field. Could you contact the manufacturer and ask them to please provide detailed charging requirements (charger voltage, current, time and temperature) for in the field recharging?
Regards,
Jeff