Other Parts Discussed in Thread: , UCC24612
Hello,
I'm attaching a schematic from a POE PD design using the TPS23756. It should be able to accept input from a 48VDC PSE or a 12VDC wall adapter. The wide input range is the reason I selected this device. The output should provide 5V at no more than 600-700mA. I tried to keep it as simple as possible in order to reduce the BOM because of size constraints. I would like to hear some opinion about this design. Please don't focus on details like g.e. the Class Selection resistor. I'm mostly concerned about the Transformer which is designed for 36-72VDC input and at 12V its power may derate considerably. Thank you in advance!