Hello team,
I use TPS61045 in my project, the schematic diagram as attached. My application conditions are as follows:
1. Input voltage: 4~5.5V, output voltage: 16~17V.
2. L1: 4.7uH LQH43CN4R7M03L; D1 MBR0530
3. I calculated TPS61045 can output 29mA max in my application,the actual maximum current consumption is ~15mA.
Could you help to evaluate the SCH is ok?
Recently I found that there are several IC which the output voltage is abnormal. The normal output voltage is ~16.5V and the current is ~ 10mA. The abnormal phenomena are as follows:
1. The output voltage of TPS61045 is ~20V, I measured output current is about 40mA.When I removed L1, the value of L1 changed from 4.7uH to ~0.1uH,the actual test load consumption is ~10mA.
2. Another TPS61045 output is ~14.5V, the output current is ~15mA, I removed L1, measured L1 is 4.7uH, the actual test load consumption is ~ 8mA, where is the excess 7mA current consumption?
I have some confusion as below.
1. What are the reasons of output voltage and current of TPS61045 are so different from the theoretical calculation.
2. After I removed the inductor L1, I replaced it with a new one and the IC worked normally.The rated current of L1/4.7uH is 750mA.
Is L1/4.7uH causing the IC work abnormally or the IC causing the L1/4.7uH damage?
3. What are the reasons that can cause the value of L1 changed?
I look forward to your analysis as soon as possible.
Thanks!
Kevin