Other Parts Discussed in Thread: TPS23731
Hi!
I was planning to use TPS23731 in a 12V, 25W design, but when I noticed that the part was not available I realized that the TPS23734 would also work with the added benefit of supporting ACF.
Can you explain the tradeoffs using ACF vs the flyback mode? My TPS23731 design is using primary side regulation and I was hoping that I could do the same using TPS23734 but the EVK is using an opto coupler instead. Is primary side regulation not recommended in ACF mode or can those be combined to improve efficiency + eliminate the need for the opto coupler?
If the opto coupler is need in combination with ACF, is it possible to achieve the same functionality as TPS23731 simply by using the same schematic as the TPS23731 EVK and connect the DT pin to GND.
Stefan