hi sir
could you help to review the schmatic?thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alex,
I have checked the schematic connections and have one comment. The AGND pin should not be connected to PGND on their board as the connection is done internally in the module. This is described in the pin functions table on page 7. After making this correction, some of the external components should be connected to the AGND pin net instead of DGND. Those components recommended to be returned to AGND are those connected to INH/UVLO, SS/TR, RT/CLK, VADJ, STSEL, OCP_SEL and ILIM.
Can you help provide some details how the external component values were selected? Was WEBENCH used?
Anthony
Looks good. One thing I noticed is they will want to use different nets for the AGND of each device. Such as AGND1, AGND2, etc. They probably would have noticed this when going to layout their board.