Other Parts Discussed in Thread: BQ25505
Hi everyone,
I'm using BQ25504 in the evaluation board (ref EVM-674) and I have a problem when my output tension is 1.77V.
I'm using a power supply limited at 0.7V and 1.5mA so as you can see in the figure below the output (in green) and bat (in blue) voltages are increasing.
When the output voltage is 1.77 (as mencioned in the datesheet) the input drops to almost 40mV and the current is the maximum. In this case I'm not using MPPT and there is not load in the output. At Bat pin I have a 1mF capacitor. In next figure I put the behavior of the input when the output is 1.77V like I said.
Do you know why is this happen ?
I have another board with the BQ25505 and I don't have this problem. One difference I saw between these components is in the PFET between BAT and VSTOR pins.
Thank you,
Lucas.