Hello team,
I want to use TPS61087 in my project.
Below is my application:
Vin:3.0~3.6V
Vout:4.65v
Iout:0.8A max
Can CCOMP be equal to 820pF?
In the datasheet Page 14:
Make sure that RCOMP < 120 kΩ and CCOMP> 820 pF, independent of the results of the above formulas.
My theoretical calculation RCOMP is 44K. I choose RCOMP =45.3K.
How to choose CCOMP? Is C=820PF ok?
Could you help to review the sch attached,please give your recommendation.
Thanks for you support.
kevin