Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8866-Q1: LP8866 flicking

Part Number: LP8866-Q1

Hi,

In emergency situations, the backlight will flash when Vin is 8V,
We use X-Ray to confirm that the status of PCB printing is OK, and the boot sequence Vin, VDD, EN are normal!

It is found that the SD Pin that controls the MOSFET will always be pulled High!

LP8866 (I2C)data is as follows

00h:0xCCCC
02h:0x0FFF
04h:0x0AA3
06h:0x0100
08h:0x2AAA
0Ah:0xA028
0Ch:0x00AA
0Eh:0x0000
10h:0x0002
12h:0x0510
14h:0x000F 
16h:0x0000
18h:0x0000
1Ah:0x01FF
1Ch:0x06F5
1Eh:0x7621

If you need SCH, please tell me