Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92200D2EVM: TPSM53603EVM switching noise

Part Number: TPSM53603EVM
Other Parts Discussed in Thread: TPS92200

Measuring noise at output DC for TPSM53603EVM 24VDC input with 5VDC output and 3A load (LED string). Want to make sure what I'm seeing is correct. Per the specs, the voltage ripple at these parameters should be 8mVpp. However, with the switching noise, the voltage ripple is actually100mVpp

Yellow is showing 5VDC output with100mV / @ 1.4mHz 

Just want to make sure what I'm seeing is normal. I can add LC low pass filter on the I/O lines if needed to be since I'll be feeding the output to MCU.