Hello,
Our customer asked VFB voltage min, max value at CCM condition, ever since he could see these number in Skip mode but could not see in CCM in the datasheet.
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Our customer asked VFB voltage min, max value at CCM condition, ever since he could see these number in Skip mode but could not see in CCM in the datasheet.
Best regards,
Hi Imi-san,
In datasheet, it marked as (1) which means this data is ensured by design. Not production tested. We don't have the min and max value of VFB at CCM condition.
You can refer to Skip mode. They are familiar or CCM is a little bit smaller than Skip mode.
Thanks,
Lishuang
Thank you for your reply.
I understood Vref tolerance in CCM is similar or slightly lower to Skip mode, that is 0.7000V +/-0.5% @Ta=25C, 0.7000V +/-0.8% @Ta=0C to 85C, 0.7000V +/-1.0% @Ta=-40C to 85C.
best regards,