Hi, in error I have only grounded pin 3 and the thermal pad for this part, but failed to ground pin 5. This is causing the regulator to produce 2.2V instead 1.8V. I currently have the VDDIO pin of a DS90UB925 connected to this regulator that can handle 1.8V +/- 5% or 3.3V. IDDIO is 1.6mA (Max). It currently does not use any outputs only its inputs and where V input high is 0.65 * VDDIO. The inputs to the DINX pins of the DS90UB925 are 1.8V. Here are my questions:
1) Given the low load current of 1.6mA (Max) on the regulator, can I expect the regulator to be stable at 2.2V even though pin 3 is not grounded?
2) Should I be worried if I supply 2.2V to the VDDIO pin of the DS90UB925 even though it is outside of the recommended voltage range, but still well below absolute max?
Everything is currently functional, but I am considering if there could be any long term repercussions.
Thank you,
JP