This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40190: Busted Chip - is it this device?

Part Number: TPS40190

Image from a board with a busted chip.

24V was applied to the system, and there were some fireworks. This chip has a hole, and the "0190" marking code seems to align with the TPS40190. The device ABS MAX is also only around 16V, so it makes sense we might see fireworks at 24V.

This chip is the TPS40190 - right? I am pretty sure, but just hoping for some verification.

Thanks!