Other Parts Discussed in Thread: LM2596, LMR33630
I am bringing up a new board using the LM2594MX-5.0/NOPB using recommended component values per Webench Power Designer.
This is based on 20VDC-30VDC input range with 24VDC being nominal. Design is based on 500mA max on-demand current with 150mA typical. I can provide a BOM if needed.
The regulator output voltage consistently overshoots on power up. This event peaks at close to 10V and stays above 5V for over 3mS. I believe this may be damaging a downstream LDO regulator with a 6V max input voltage.
Lower Y cursor represents nominal 5VDC output, upper Y cursor is the 9.89V event peak, span of the two X cursors represents the initial rise above 5V to voltage stabilization)
I have only observed this on power-up and the voltage is steady at 5V +-50mV afterwards. This has happened consistently across 3 PCB assemblies
I've used variations of this same basic design in several products with great success and this is the first time I've seen this.
A zener diode at the output is effective at clamping the voltage however I'd prefer address the root cause if possible.
Has anyone else resolved a similar issue? Any suggestions or thoughts are appreciated.
Best Regards,
JLP