Dear Team
Good day!
I had check the tps63900 datasheet (Rev.D) and found some contradictory information . please correct me
In the datasheet , chapter 6.3 ,it shows the output current is 0.4A(Max) , but from the Figure 8-2 to Figure 8-7 , the Typical Output Current Capability versus Input Voltage can reach 1A , it shows many test graph base on the 1A output current .
1.Does the tps63900 can support 1A (Output current)?
2.if the output current in the test result actually is the peak current value . could you tell me how long could the peak current last.
Best regards
Leon.liu