Hi,
I am using BQ25792 in my application to charge the 3S1P Li-Ion Battery Pack. The charger IC which is working well and communication with the host controller are all fine. But the problem is the BQ chip is heating even there is the battery is not connected. It consumes 60mA at the source side without the battery connected. While charging the battery at 1A, the chip temperature goes to more than 100 degrees Celsius. Help me to solve the problem....
Input Voltage: 12VDC
Charging Voltage: 12.45V
Charging Current: 1A
Regards,
Nishanth M