This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25890: BQ25890 design and Register question

Part Number: BQ25890
Other Parts Discussed in Thread: BQ25895

Please help to Schedule review as attached.

My setting as blow

Battery is 1900mA

Input 7.6V/3.25A

Battery_Volt want to charging 2A

BV_vol need 4A~5A (include Battery Dynamic Power Management)

We want to used it without USB interface and only power input at 7.6V/3.25A, is it ok ?

If no, which chip can we use ?

If yes, which Register should I set ?

My set Register as blow, please help to check enough or not

REG00[7:0] = 01111111

REG02[7:0] = 00110100

REG04[7:0] = 00100000

REG0E meet I can get real battery voltage right ?

REG12 meet I can get real battery charging current right ?

REG13 I want to have Dynamic Power Management, how should I set ?

others used default.