Other Parts Discussed in Thread: BQ25895, ,
Hello all,
I am using TPS61253 Boost IC to boost 3.8V from 375mAH Li-Ion battery to operate a load of 2A and also charge the backup Li-Ion battery of 115mAH using BQ25895 chip. Looks like battery is not able to deliver the necessary current and the load circuit does not boot up correctly. Is there a way to fix this issue?
If I use an external supply at 4.7V and 3A. the complete circuit works, charges the backup battery and is stable. So I am guessing the issue is the current limitation from the 375mAH battery.
Appreciate if anyone could guide me to the correct way of doing this.
Regards,
AJ