Hi TI Team,
I am looking a BUCK Regulator with efficiency near by 95% or more.
Input Voltage - 12V
Output Voltage- 5V@4Amp
Efficiency - more than 95%
Heat sink is not required in the system.
Please suggest the suitable parts.
Thankyou
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Abhishek,
TPS565201 can meet efficiency requirement. Please see below simulation result with Webench.
BRs,
Edwin.
Hi Kumar,
I checked that TPS566231 efficiency under 12Vin-5Vout-4A can be up to 94.9%, under 12Vin-5Vout-3A can be up to 95.2%. You can check the datasheet or request an EVM on TI.com to evaluate.
Thanks,
Lishuang