Hi,
We have uploaded required .zip file to get Chem ID using GPC tool.
Steps we have followed to generate .zip file is
1)Charge the battery to its maximum voltage
2)Relax for >2Hrs
3)Discharge the battery till it reaches termination voltage (9V)
4)Realx for > 5Hrs
GPC report shows the best Chem ID as 3608 which is Obsolete and tells use 2088 instead. If I check 2088 Chem ID, which is NiCoMn/carbon (4539mAh) model.
We are using Lithium Ion NMC 3s1p battery with each cell voltage 3.7-4.2V with 2900 mAh capacity.
1) We wanted to confirm that, is Chem ID we received from GPC tool is matching our battery configuration or we have missed any steps while capturing the log(rel-disch-rel) cycle which led to wrong chem ID.
2) If chem ID is matching our battery configuration, then should we use 2088 as chem id?
Please find the attached .zip file and GPC report we received.
ChemIDgenaration.zipChemIDgenaration-report.zip
Please guide us on this so we can complete learning cycle with proper Chem ID.
Thanks and Regards,
Sudha Nayak