Other Parts Discussed in Thread: CSD18563Q5A
When debugging LM5117, we found that the input voltage is lower than 45V, and the output is only 15V(issue). If we increase the voltage to 50V, the output is ok (normal output voltage is 23V), and then reduce reduce the voltage to 26V, the output is also ok.