Other Parts Discussed in Thread: BQ33100, , EV2400, BQSTUDIO
Hi,
I'm using the BQ33100EVM-001 and EV2400. I have just flashed the BQ33100 firmware to the latest version. Device is shown as bq33100 R0, FW version V0_15_BLD0017
I have 5x 100F, 2.7V, 15mOhm super capacitors wired to the EVM.
My EVM is connected to a 14V PSU.
The board is running but i wanted clarification on some of the settings.
I've carried out a Capacitor Voltage Calibration, with the voltage increasing by 2.1V (2100mV, 4200mV, 6300mV, 8400mV and 10500mV.
- On the System Voltage Calibration the measured system voltage is shown as 13991mV but the actual system voltage is shown as 2000mV. I don't appear to be able to change this, such that its saved. it always reverts back to 2000mV.
- In SBS the capacitance is reported as 2.0F and ESR 400mohm.
- In Dataflash>System Data the Design Capacitance, Init 1st Capacitance and Capacitance are all 2.0F. How do i change these to reflect the capacitance used? What is the difference in the three items?
- In Dataflash>System Data the Design ESR, Initial ESR and ESR are all 400mohm. How do i change these to reflect the ESR of the capacitors used? What is the difference in the three items?
- In Dataflash>System Data the Design voltage is 9000mV. What is this value referring to?
- In SVS in the safety status i see a OV flag set. Why?
Thanks.