Please let us know pin treatment of SYNC_OK pin at standalone operation.
SYNC ---> connect to GNDP
SYNC_OK ----> Pull up to VINP ?
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kura,
SYNC_OK is an active LOW, open drain, output that can be connected directly to VINP if SYNC/SYNC_OK are not being used. If SYNC is driven externally and the possibility of SYNC_OK transitioning LOW exists, then a pull-up resistor of >10 kΩ should be used between SYNC_OK and VINP. Thanks for connecting through E2E and please connect with me through email so I can understand more about the project you are working on: s-mappus@ti.com
Regards,
Steve M