Hi team,
Please find some customer feedback below. Are these actual errors or is there a misinterpretation?
I have gone through the data sheet of the TPS717. I noticed two things:
- Section 8.2.2 (page 18 below) describes how to design the resistors for the feedback divider. Equation 4 is linked here. Shouldn't this be Equation 3?
- Section 8.2.1.2 describes in detail how to dimension the feedback divider. With the given equation I cannot reproduce the values in the table below. I think the "-1" does not belong under the fraction but behind it. So R1=R2*((Vout/Vfb) -1)
Thank you,
Franz