Other Parts Discussed in Thread: LM5170, LM5156
Hi team,
Can LM5170 support 5V to 60V boost with 15W?
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
The answer is yes if your switching frequency is less than 300kHz. The available max duty cycle is (1 - 250ns x Fsw). However, it appears to be an expensive solution for just 15W.
Instead, could you consider the LM5156 operating in DCM such that it can support without hitting the max duty cycle? Which sounds like a much better cost effective solution.
Thanks,
Youhao Xi, Applications Engineering