Other Parts Discussed in Thread: UCC12040, , SN6501-Q1, UCC12050
Hi team,
Could you tell me which internal transformer driver circuit is used and how it operates?
Is it as same as SN650x?
Regards,
Ochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could you tell me which internal transformer driver circuit is used and how it operates?
Is it as same as SN650x?
Regards,
Ochi
Hi Ochi,
UCC12040, UCC12050 and UCC12051-Q1 are unique compared to SN6501-Q1. SN650x is an open loop (unregulated output voltage), push-pull driver with integrated MOSFETs, operating at frequencies up to 410kHz and driving an external isolation transformer and secondary side rectifier. UCC12051-Q1 is a fully integrated, closed loop DC/DC converter module that includes primary and secondary side MOSFETs, isolation transformer and a regulated isolated secondary side output voltage packaged in a 3.5mm high, 16-pin, SOIC. The 8MHz frequency of UCC12051-Q1 is necessary to reduce the size and profile of the transformer. UCC12051-Q1 uses several proprietary control and transformer design techniques aimed at reducing EMI, enabling certification to CISPR 25, class 5. Please email directly for more details: s-mappus@ti.com
Regards,
Steve M