This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25150: Bq25150

Part Number: BQ25150


Hello team,

Am presently working on bq25150,am facing an issue regarding battery regulation voltage at BAT pins.

1.here am not getting 4.2v battery regulation voltage at,

My BAT pin,in my schematics my CE pin left floating and,

And configured ce to low for charging to enable,am getting 1.9v at my

Bat terminals,what is the reason..?

2.Is ADC need to be configured,for battery charging,

If yes,what are the registers need to be configured

3.Is bq studio supports only for interfacing eval boards of bq25150

As am using bq25150 ic in my hardware, can i able to capture the data using any tool ,is it supports..?

If it supports,plz provide me with that tool,it will be helpful..

Thanks in advance

Suraj.n