Other Parts Discussed in Thread: TPS546D24A
I have about 800uF of output capacitance. VOUT is 1.2V
My VR is configure to power on/off based on the operation register.
When I power down it takes about a minute or so to go below 100mV. Is there a register or setting that can pull this voltage down faster?
Also, as a workaround, I tried setting the voltage to 0V, but it will only go as low as 500mV. What could be the reason why my voltage won't go lower?