This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3880: Incomplete Sequence Operation

Part Number: LM3880
  • Hello

    1. we are checking whether these number are available.

    2.  For LM3880MF-1AA, the the power down stars 10ms after the enable is de-asserted. with 120ms period, it gives enough time for the device to complete the power down sequence.

    Regards

    Yihe.

  • Hello

    Since the 120ms is from the same clock/timer as other timing parameters, it will follow the same variations defined in the data sheet. for LM3880MF-1AA, it is 15%. 

    Regards

    Yihe