Dear TI Team
I have something to check about TPS62901.
When I checked the following New product update materials, TPS6290x was introduced.
About the advantages of TPS6290x The document states that it can be implemented with a Single-Layer PCB layout.
I would like you to answer the following about this.
1. Is it correct to recognize that using TPS62901, it can be mounted with only a single layer including GND and heat dissipation parts?
(Usually, when mounting a DCDC, we think that it will be mounted using multiple layers as a measure against noise and heat dissipation. If it can be mounted with only a single layer, we think that the cost of the board will be greatly reduced.)
2. It is said that it can be configured with only a single layer. Is it possible to mount it on the back side of the component side, for example?
(I think that mounting with only a single layer means that it can be mounted on the back side of the surface on which other parts are mounted. This can reduce the board size.)
Best Regards,
Y.Ottey