Other Parts Discussed in Thread: LM5145, , CSD19534Q5A, CSD19533Q5A
We are using LM5145 this part with the low side FET (NTMFS015N10MCL) and the high side FET (FDMS86102LZ). However, the output voltage was abnormal. so we would like to know if there is any recommendation on the FETs to replace NTMFS015N10MCL and FDMS86102LZ. I found CSD19532Q5B is pretty much equivalent to NTMFS015N10MCL, but still would like get the recommendation.
Here is the application:
Input voltage range: 24~ 60 V
Output voltage: 12 V
Output current: 4~5 A max
Target topology: buck
Thanks.