Hi Experts
My customer is creating the following TPS546C20A design in WEBENCH® POWER DESIGNER .
TPS546C20A buck regulator in WEBENCH, Vin min = 5V, Vin max = 5V, Vout = 3.3V, Iload = 6.5A max, Iload min = 6A.
Here are the problems being reported:
- For some reason it is not allowing me to select a switching frequency of 700kHz.
- Also I used the datasheet to calculate the switching inductor value, however the WEBENC tool generated a design with a different size inductor.
Best regards,
Jim B