Hi Team,
Can you explain to me under which conditions the Iq was measured for BQ25570?
Under electrical characteristics (page 6) it says that VIN_DC is 0V for all Iq typical characteristics.
Can you please explain this?
BR,
Stefan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Can you explain to me under which conditions the Iq was measured for BQ25570?
Under electrical characteristics (page 6) it says that VIN_DC is 0V for all Iq typical characteristics.
Can you please explain this?
BR,
Stefan
Thank you Jeff for your fast reply on this!
One additional question:
What if Vstore=0V, Vbat>=2V, /EN=’0’, how much will it consume? Can I consider also here the 800/900nA? Will this also be taken from the battery, right?
Stefan,
If VBAT>2.1V, the PFET between VSTOR and VBAT turns on so that VBAT can power VSTOR, including the Iq of the charger itself.
Regards,
Jeff