Hello,
I was looking at recommending this TPS54218 EVM for a customer to test the TPS54218. However, they would like the ability to change the switching frequency flexibly between the 300 and 2000 kHz range and output voltage and current to 0.95 V @ 0.36 A. Would it be feasible for the customer to change these external components on the physical EVM to test these specs?