This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3658: Charge STAT error

Part Number: LM3658


Hi all. I used LM3658SD-A/NOPB with TS pin disabled. STAT1 and STAT2  1Hz-blinking when AC wall adapter connected whitout battery. Is that right?It seems not described in datasheet. Best regards

  • Hello,

    If both STAT1 and STAT2 are on this indicates the pre-qualification mode aborts, you can see more in datasheet section on titled "pre-qualification mode"

    Thanks,

    Nick

  • I see, but I think  ‘ON’ means constantly. Here is the video with adapter connected without battery

  • Hi,

    You can refer to Table 1. Status Pins Summary

     

    Best regards,

    Nick