Hello team,
can you confirm if we can regulate the output voltage with the Rset resistor? We tested it with the EVM (modified), it works well. The config makes sure the FB current should not get larger than the recommended 100uA.
We have 12V on input and want to be able to configure output to 18V, 24V, 30V, 36V (with ability to change while device is operating).
I can share the schematic of the EVM modification offline.
Thanks