Dear TI Team
When I carried out WEBENCH under the following conditions, the following circuit came out.
Vin = 4.75-32V
Vout = 3.75V
Iout = 1.5A
At this time, if you check the voltage applied to the EN terminal from the voltage dividing resistor connected to the EN terminal when Vin = 32V,
32 × 44.2k / (105k + 44.2) = 9.47V
I think this exceeds the absolute rating of the EN terminal, 5V.
Is it okay to set the voltage divider resistance of the EN terminal as in the circuit above?
(If there is no problem, please tell me the reason.)
Best Regards,
Y.Ottey