Dear TI Experts,
Refer datasheet: SLUSCA8A –FEBRUARY 2016–REVISED FEBRUARY 2016)
I need to calculate the shortest Tdemag (time when the UCC28704 will sample the Vs pin after turn-off of MOSFET), refer datasheet Fig 14. Of course, in an existing simple DCM flyback with known components, this can be easily calculated once we know the minimum MOSFET current at turn-off, which can be calculated from the minimum turn-off voltage at the CS pin, and value of resistor Rcs. Datasheet Table 6.5 states that minimum CS turn-off voltage is 170mV. However, what I do not understand at this time is how the resistor RLC modulates this turn-off voltage (refer Fig 24). Please advise how to calculate the minimum MOSFET turn-off current from the components of Figure 24, taking into account RLC
Regards,
Jonard Rico