Part Number: TPS63021
Other Parts Discussed in Thread: TPS63020
Dear Sirs,
We want to use TPS63021 chip in our design. As I understand from datasheet TPS63021 contains internal divider on FB pin. The electrical characteristics show that TPS63021_FB input impedance (apparently, sum internals R1 + R2) is equal 1MOhm.
I have some questions about TPS63021:
- Can I add an additional resistor Rext between FB and Vout pins to change the output voltage level (Vout)?
- What is the range of Vout can I set with the help Rext between FB and Vout pins?
- Can I set Vout = 3V3? What is Rext value I should set between FB and Vout pins for Vout = 3V3?
- What are the values of the Rup and Rdown resistors at the FB input (pin) inside TPS63021 chip (figure 4. Functional Block Diagram (TPS63021) of datasheet)?
- Can I set Vout voltage with the help Vout = Vref * (1+ (Rext + Rpu) / Rdown)) equation? Where Vref = 0.5V, Rext - resistor between FB and Vout, Rup and Rdown resistors at FB input inside TPS63021 chip. Is it correctly?