Hi, there
I am using bq24725a with Linux on iMX processors, just wondering is it possible to disable the power source from battery (BATDRV) without adaptor plugging in?
From the datasheet, I only found that we can switch power source if there is adapter detected. I am trying to read the battery voltage and turn it off if the voltage is lower than some level, even if there no adapter attached.
Also, the LEARN mode is not working as expected. The power source got switched from battery to adapter if I plug in the adapter, but the battery level is higher than 70% which is the battery depletion threshold I set. Is it suppose to continue using the battery power source until the voltage lower than 70%?
Regards,
Jacob