CSD15380F3: Which is the 1 pin?
Below is datasheet:
Below is CAD/CAE file:
Which is correct?
Please reply to me as soon as possible.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CSD15380F3: Which is the 1 pin?
Below is datasheet:
Below is CAD/CAE file:
Which is correct?
Please reply to me as soon as possible.
Hi Mickey,
Thanks for your interest in TI FETs. The drawings in the datasheet are correct. When viewed from the top, pin 1 is in the upper left corner as shown in the recommended PCB layout. The mechanical drawing showing the pin locations on the package is viewed from the bottom with the package flipped over and pin 1 is in the lower right corner. It appears that the footprint produced by Ultra Librarian has pin 1 and 2 swapped. Apologies for any confusion. The datasheet always takes precedence over the other documents.
Best Regards,
John Wallace
TI FET Applications