Other Parts Discussed in Thread: TPS62160
It is designed to output 3.3V by receiving 12V input using TPS62160.
For the feedback resistance value, 470K and 150K were applied, referring to Figure 7. 3.3-V / 1-A Power Supply in the Datasheet.
Regardless of whether there is an output load or not, all of the produced development boards are measuring 3.22~3.27V, which is lower than 3.3V, so we ask to confirm whether the measured values are within the normal range.
When measuring FB voltage, it is measured around 0.77~0.78V.