Hi team,
We are using the Texas Instruments LMG1020-EVM-006 evaluation board to drive the laser diode. The attachment shows the results of experimental result. Yellow line shows the pulse pattern given to the EVM board by FPGA. Blue line is measured at monitoring port after gate driver which shows oscillating result with around 18ns between adjacent peaks. Yellow line is the measured output of the laser diode which also shows multiple peak result. The pattern generated by FPGA is 50kHz and 180ns. Can you comment on the oscillation measured at Gate voltage and laser output?
Best regards,