Other Parts Discussed in Thread: TPS61500
Dear TI Team
I am looking for an LED driver that meets the following conditions
・ Constant current boost type
・ VF: 6.15V (TYP)
・ Number of series: 1 (Use this LED (2 LEDs in series) in 1 row)
・ Required supply current: 1.2A (up to 1.5A if more current can flow)
・ Input voltage: Li-ion battery voltage (2.7V ~ 4.2V)
I searched for an LED driver that meets the above, but it wasn't on the web.
Are there any products that will be released in the future that meet the above conditions?
Best Regards,
Y.Ottey