Because of the Thanksgiving holiday in the U.S., TI E2E design support forum responses may be delayed the week of Nov. 21. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61169: About the lineup of step-up LED drivers

Part Number: TPS61169
Other Parts Discussed in Thread: TPS61500

Dear TI Team

I am looking for an LED driver that meets the following conditions
・ Constant current boost type
・ VF: 6.15V (TYP)
・ Number of series: 1 (Use this LED (2 LEDs in series) in 1 row)
・ Required supply current: 1.2A (up to 1.5A if more current can flow)
・ Input voltage: Li-ion battery voltage (2.7V ~ 4.2V)

I searched for an LED driver that meets the above, but it wasn't on the web.
Are there any products that will be released in the future that meet the above conditions?

Best Regards,
Y.Ottey